This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

at OMAP35xx there is an option to boot as a USB device. We found out that there may be some initialization code that could be interesting for us.

Other Parts Discussed in Thread: TPS65920

At OMAP35xx there is an option to boot as a USB device. We found out that there may be some initialization code there we do want to see. As far ad I understand this code is placed on production at the OCM (On Chip Memory).

In general it seems that we are missing something with the OMAP35xx and PMIC TPS65920  initalization - the code should initialize the PMIC OTG MODE this is writing 0x20 OTG_EN  to POWER_CTRL_SET register.

Is there a way to get the sources of that OCM ?

Anything additional suggestion is appreciated!

 Micha