Hi,
I have a question about VTTP_ 100 of DP83848IVV.
The following is DC specification of VTTP_100.![]()
Is this measured differentially after 1:1 transformer?
Or is this mesuared TD+/TD- signal output?
I think this indicates the specified value after transformer(1:1).
As you know, the IEEE 802.3 specification defines the required 100BASE-TX VOD (Voltage Output Differential). Per the specification, this voltage must be 1V +/-5%. So, 0.95 to 1.05V. the transformer(magnetics) have ±2%. If TD+/TD- is 0.95 to 1.05, it is fail for the IEEE 802.3 specification. (the VOD becomes 0.931 to 1.01)
If we obseve the following conditions, the output of RJ45 becomes 0.95 to 1.05V and it pass the compileance test for VOD.
- RBIAS = 4.87 kΩ 1%
- Transformer(Mangnetic) = 1:1 2%
Is this understanding correct?
Best Regards,
Taka