This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SNx5DP159/TMDS171/TMDS181 EyeScan control register

Hi,

Glad to see the data sheets recently updated. Still, there are some things which does not seem clear enough. In particular:

Each the part implements the Rx Pattern Verifier Control/Status register. The register has PV_LD[3:0] field which is defined as follows:

PV_LD[3:0]. Load pattern-verifier controls into RX lanes. When asserted high, the
PV_TO, PV_SEL, PV_LEN, PV_CP20, and PV_CP values are enabled into the
corresponding RX lane. These values are then latched and held when PV_LD[n] is
subsequently deasserted low. 1 bit per lane.

Please clarify what's the PV_TO field mentioned

---

regards,

    Igor

  • I suspect there is no PV_TO field. It seems the whole text is derived from the description for corresponding field of the Pattern Generator Control register (PG_LD[3:0]). Indeed there is PG_TO bit. As for the PV control register, looks like the respective bit is merged to the PV_SEL[24:0] field ("1xx - Timing only mode with sync pulse spacing defined by PV_LEN"). By the way PV_SEL[2:0] would be the better name for the field, I think.

    Any comment?

    BTW one said careless documentation frequently linked to careless implementation. No wonder there is the bug in silicon.

    ---
    regards,
    Igor

  • Hi Igor,

    You are right, PV_TO is a typo, this field doesn't exist.

    Regards