Other Parts Discussed in Thread: DP83848C, DP83848I, DP83848YB, DP83848VYB, TPS5401
Hi everybody,
I have a problem for a while with the ethernet part of my electronic card.
I have a STM32F207ITG which is wired to the DP83848CVV. I have used the same wiring as the one on the evaluation board MB786 of ST (link). You can see my wiring here.
I have used the STMCube to test my card in a first time. Without the Ethernet part, I know that my µc is working well (I can change status of inputs, outputs...). But, the only thing of plug in an Ethernet cable into the RJ45 connector reset my board (but without any initialization of Ethernet in my software).
I can see it, because, the two LEDs on the RJ45 connector start to blink and then switch off (a little video is available here).
So I don't understand why the fact of plug in an Ethernet cabe reset my board. If you have any ideas or suggestions.
Thank you in advance,