This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9517A MAX vILC

Guru 16770 points

Hi

Do you have information about the max/min value of vILC?

Or can we estimate these values?

Best Regards

  • Hi,

    We provide the typical value of VILC in the datasheet (see image below):

    We do not provide min/max because  the difference of VOL - VILC will equal 0.5V which is the offset that is shown on the B - side of the device.

    Thanks,

    Siby