Other Parts Discussed in Thread: TPS65982, TPS65982-EVM
Hi
Our customer is going to evaluate TPS65982EVM.
The customer configuration is the following;
A. The connections
- The one TPS65982 is set the DRP mode(Conf ID#: 2) --> supply side
- The another TPS65982 is set the UFP mode(Conf ID#:7) ---> receiver side
B. The power supply
The power supply is connected directly with the wire to the pattern of PCB because the AC Adapter which is include the EVM is not suitable in Japan.
The questions are;
1. Is that possible to set with the above(A.) configuration?
Our customer set the above configuration to evaluate the DRP and UFP operation with the two EVM.
However the DCDC which is U7(TPS54335) on EVM(DRP mode) is broken.
2. Is the following connections possible?
Regards,
Koji Hamamoto