Other Parts Discussed in Thread: TPS65982-EVM, TPS65982, TPS6598X-CONFIG
Hi,
I'm using 2 TPS65982-EVM boards, connected together with USB C-C cable, one as Provider (CFG ID #2) and one as Consumer (CFG ID #7).
After power contract done, and VBUS is 12V, if I press Reset button on Consumer board, it just stops working. VBUS is still 12V but no more LED on, no power output at PPHV. I also notice that right after Reset button is pressed, LED B blink once then turn off. Thing only becomes normal again if I unplug the cable or reset Provider board.
It does not happen if I select 5V power mode, for example Consumer with CFG ID #4. However, in this case, the Consumer board does automatically self-reset once again after I release RESET button about 1 ~ 2 seconds.
So is it correct that after reset, TPS65982 requires 5V VBUS for normally operation? Please help to check, thanks.