Other Parts Discussed in Thread: HD3SS6126
Currently doing a design using a HD3SS6126RUAR in the uplink path of a TUSB8041IRGC Hub. Port A connected to Hub uplink.
It allows the switching of USB2.0/3.0 from the Hub to two different connector points via ports B and C
Datasheet for HD3SS6126RUAR seems to indicate that signals need to be AC coupled in/out of sides A, B and C, however the evaluation board for HD3SS6126 shows no signs of AC coupling at all.
Since this is just a switch is there a need to AC couple between the Hub uplink and switch port A since this is inside our system ?
Ports B and C will AC couple on Tx pairs as this is to the outside world and Rx pairs on ports B and C will Ac couple at the host ends.