Other Parts Discussed in Thread: TUSB2036, TPS2042, TPS2052
Hello,
I am designing a 2-port USB hub using the TUSB4020. I successfully used the TUSB2036 before but our new application requires a USB 2.0 hub.
I followed the datasheet design recommendations and got the TUSB4020 to connect to my PC, it is recognized as USB 2.0 MTT Hub. However, I seem to have a problem with downstream ports.
I tried two different switches: the TPS2042 and TPS2052, changing the PWRCTL_POL pin to active low and active high respectively,
I noticed that the PWRCTL2/BATEN pins are always pulled high ( 3.3V ), regardless of PWRCTL_POL .
I attached my schematics for your reference. I appreciate any idea or help in identifying the source of the problem.