Hi there,
We need these converters to extend the distance of RJ45 cables. Now we are using a 3-rd party product, which works in physical layer (layer-1) with a latency of 0.9us. but the reliability of this product is a big issue. So we are wondering if we could build this product ourselves with TI chips, like DP83849 series. I just had a look at the some datasheets and also the evaluation board, but i am not very sure about this, especially the type of fiber port supported, (i.e., single-mode, multi-mode).
BTW, we only need one RJ45 port and one Fiber port for each device. they are both 100mbps, full-duplex. In addition, one single fiber to connect a pair of these converters is preferred, such as 1310nm (wavelength) at one side, and 1550nm at the other side.
Since i am new with this, so more details and information are greatly appreciated:) Thanks.
Best Regards,
Circle