This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it available to use DS90UH947 and UH948 without Open LDI mapping?

Hi,

 I have a basic question. I am using combination of DS90UH947 and UH948 with Open LDI mode and dual mode.

 Is it available to input and output as simple serdes I/F without relationship of Open LDI? It means that it is used to input from D0 on UH947 and output to D0 on HU948, D1 on UH947 to D1 on UH948, D2 on UH947 to D2 on UH948, and so on  without  Open LDI mapping.

Best Regards,
Kenshow