Other Parts Discussed in Thread: TS5A63157, TPD1E04U04
Hi,
I'm using the TS5A63157 in the first stage of a guitar amplifier to provide a -10dB attenuation option. I have had a couple of failures of the device - the nature of the failure is that it still passes the analog signal but looks like a 10K approx. impedance. The circuit diagram is below:
VCC5.5 is supplied from a TPS7A4901 LDO. VGND is VCC5.5/2. D3 is a 5V TVS bi-dir diode. VCC5.5 is switched on after the MCU detects a guitar is plugged in. VCC5.5 is switched off if there is no input signal for N seconds and switched on again if an inout signal is detected.
In the case of failure, the circuit still works in the sense that analog passes through the device but the change in effective input impedance drastically lowers the signal level so that the audio detect no longer works unless you hit the guitar really hard.
Is there anything additional that I should do in terms of device protection? The TVS diode will allow an ESD spike to hit the TS5A63517 of approx. +/-5V. I've checked some of your reference designs that use this device but none of them have a device near an input terminal.
Appreciate any advice.
Kind regards,
AC