Other Parts Discussed in Thread: TSB81BA3E
For TSB81BA3E, what is the recommended connectivity of PLLVDD-core and DVDD-core pins when internal regulator(s) are used, with VREG_PD pulled to ground? Should all PLLVDD-core and DVDD-core pins be tied together respectively, then connected with a ferrite bead between the two voltages?
At least one other thread (294998) poses a similar question but without a definitive answer, but only says there are two separate internal regulators.
Also, is there a reason to NOT use the internal regulator(s)? Would an external regulator be superior in some way?