Other Parts Discussed in Thread: XIO3130
Hello,
I am having an issue with the XIO3130. It is connected to PCI2 channel 2 of an upstream PCIe host port. Channel 0 and 1 go to miniPCIe cards. Channel 3 goes to an Intel I210 NIC. I need the WinRom and Top Hat tools and the normal mode and express card *.dat files
Company DDC Corporation
Address 105 Wilbur Place Bohemia NY 11716 USA
company Representative requesting tools - me, Richard Walsh walshr@ddc-web.com (631)567-5600 x 7587
Application Small rugged computer
Market Aerospace
Here is a block diagram of my implementation:
These are my symptoms. As long as nothing is plugged into the miniPCIe slot associated with computer PCIe 1, everything works fine. I see both nics, the switch (as four bridges) and the Exar card. If any miniPCIe card is plugged into the lower miniPCIe slot in the diagram, the NIC downstream of the XIO3130 disappears, though all three downstream bridges are seen. The second NIC is alive - the phy blinks link and activity. I have eliminated power and any possible board defects.
My computer has 4 GB of DDR3 and is not expandable.
Thank you.
PS: cis_apps_support@list.ti.com is a dead email address.