Other Parts Discussed in Thread: TCA8418
Dear All,
In our project the controller needs to control 3 LEDs and a 4X4 keypad. It doesn't have many GPIOs but have I2C interface. So we are looking to use the TCA8418 to do both jobs. My questions is:
(1) Can we use both the keypad scan and GPIO feature in a single TCA8418? The LEDs are always flashing to give user indications while the keypad entering happens at some times only in the running. But I am sure the LEDs flash as well while the user entering some information through the keypad.
(2) If the way above doesn't work, can we use two TCA8418s, one for LEDs and one for keypad? I understand from the datasheet that the device address if fixed.
Thank you
Trevor