Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2551A and OMAP3530

Other Parts Discussed in Thread: TUSB2551A, OMAP3530

Hi,

I want a USB 1.1 transceiver to hook up to an OMAP3530 processor, so I'm looking at the TUSB2551A transceiver.  I'm just not clear which signaling method to specify for the OMAP.  Is it 4 pin DPDM or 3pin DATSE0 signalling?

Also the TUSB2551A datasheet doesn't say anthing about pull downs on DP/DM, are these needed?

Thank you