Other Parts Discussed in Thread: LMH1980
Good day,
I am using the LMH1980 in a design which requires the input to survive a 50V 5 ms surge.
Does the AC coupling through a 100nF capacitor as per the reference design provide sufficient surge reduction to protect the LMH1980? If not please provide an indication of the surge energy that can be absorbed through the input pin voltage being higher than Vcc+0.3V without causing damage to the LMH1980.
Thanking you in advance
David