Other Parts Discussed in Thread: TCA6416A
Hi there,
I am trying to use a TCA6416A in my design. I want to be able to insert a fault on an analogue voltage, but otherwise measure with a separate A/D port the analogue value. I am using the TCA6416A as inputs which is working correctly except the VCCP power pin is drawing increased current when the analogue voltage is about mid rail. Otherwise the part is working exactly as I hoped with the outputs selectable when required.
My question is, is this correct behaviour for this device? Appreciate I'm using it outside of the designers intent, but I didn't think an analogue voltage on a digital input would cause this type of issue...
If this part is not suitable for this is there anything else TI can offer for this application?
Graham