Other Parts Discussed in Thread: TPD12S016
Our customer has a question about TPD12S016.
I'm posting the question for the customer:
++++++++++++++++++++++++++++++++++++++++++++++
Are the following values correct ?
In the datasheet: SLLSE96F;
p.6, 6.3 Recommended Operating Conditions
VIL [SCL_A,SDA_L VCCA=1.1Vto3.6V] : "0.082xVCCA" V (MAX)
VIL [CEC_A VCCA=1.1Vto3.6V] : "0.082xVCCA" V (MAX)
p.8, Electrical Characteristics (continued),VOLTAGE LEVEL SHIFTER – HPD LINE (x_A AND x_B PORTS)
VOHA [IOH=-3mA,VI=VIH, VCCA=1.1Vto3.6V] : "VCCAx0.07" V (MIN)
--
p.6) I think Low-level input voltage is typically "0.2~0.3xVCC". Those are too small.
Even the VOL of TPD12S016/SDA&SCL is "0.17xVCCA" .(p.7
p.8) It should be "VCCAx0.7".
++++++++++++++++++++++++++++++++++++++++++++++
Thanks in advance.
Best regards,
Takishin