This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI800 issue



Dear Team:

  In DS80CI800 datasheet,

Could I always force RXDET to high for 50 ohm? What's the side effect?

  • Hi Thomas,

    The RXDET circuit is generally  forced to 50 ohms in non PCIe applications.  SATA/SAS or XAUI are some examples.

    For PCI Express I recommend using automatic RXDET functionality if the system configuration is supports "hot plugging" and/or contains an Add-In-Card slot which can be populated with different lane-width PCIe functions.  Only lanes with a valid PCIe endpoint should be terminated, lanes without a valid endpoint should be left floating so the root complex can properly configure the system.

    Regards,

    Lee

  • Dear Lee:
    THank you.
    Our customer reply it as below.

    ======
    I saw Gen3x8 link in one of 162 AC power cycles. Do you think it is worth trying it to force RXDET to high? If it works,could I always set it to high? In most cases, it can be gen3x16 but there is still low link width.So,I shouldn't use "stably".
  • Hi Thomas,

    RXDET can be tied high if you can assure in your system that a receiver will always be present. The main purpose of the RXDET pin, in addition to the comments Lee made above, is in situations where a hot-plug event may occur between the repeater Tx and the endpoint device.

    Thanks,

    Michael