Other Parts Discussed in Thread: TUSB7340, TPS74401
Hi all,
My customer faced with the problem about the high output current of 1.1V core supply after reset.
And the value of the current is about 1.3A-rms.
The power supply for 1.1V is bsed on TPS74401 and is the same with TUSB7340 EVM.
And USB devices are not connected.
Could you please give me any advice for resolving this problem?
The system is with reference to the circuit diagram of the EMV, Also, B8 pin is changed to NC as the datasheet stated.
Regards,
Toshi