This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

data sheet on TFP7515 LVDS part

hi this part surface mount dip is TI62C57XK G4 top row, TFP7515 second row serves as the logic interface between an lvds connector and the row and column drivers of a 5" lcd. I am trying to locate a datasheet in order to reverse engineer this small pcb. i understand g4 means lead free. and the 6 refers to the year. there is no ti lettering only the ti logo then 62c57xk which might very well be fab location and lot code, neither of interest to me. I have found ti literature back to 2001 describing min lvds and a forthcoming series of new timing controller/minilvds receivers. i have the brochure which describes the upcoming series for T-CON (timing control the output to row and column drivers) as TFP75XXX. does anyone have a datasheet or knowledge of the part or conversely a similar part that i could measure the input and timing control outputs to determine a modern in production part.

thanks

dick kessler