Other Parts Discussed in Thread: TMDS171
Hi all,
I designed a small board with TMDS171, to keep it simple I choose to use pin strap programming mode so I can save space and avoid the need of a microcontroller to program internal registers.
It works really nice in retimer mode and I would like to make it work in that way in all the data range (250Mbps - 3.4Gbps).
Seems that there's no way to force retimer mode with pin strap programming, is that right or I miss something in the datasheet?
Thank you
Regards