Other Parts Discussed in Thread: TUSB8041, TPS2546
Hi,
I'm using the TUSB8041 to create a standalone usb hub without the need for a PC. I want to plug in in one-side my phone and on the other side a thumb drive, so I can copy my pictures from my phone to the thumbdrive.
Also the hub should be used for charging with an max. of 1.5A.
My idea was to use the 4-port Hub as a starting point and simply delete everything i don't need and add everything I will need.
I've added 3 TPS2546 for charging control, to achieve a max current of 1.5A and let everything around the TUSB8041 like in the reference design.
Now my question: Because my phone doesn't connect to the thumbdrive, if booth are connected, was the TUSB8041 the right choice for this task?
Thanks and regards.