This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640 EVM act as Master?

Guru 15520 points

Other Parts Discussed in Thread: DP83640

Hi,

I have a question about DP83640EVM.
www.tij.co.jp/.../dp83640t-evk

I'm thinking to use DP83640 as GrandMaster

We are planning to get DP83640EVM and have following question:
Can DP83640EVM act as Master?
We are planning to connect Slave against DP83640EVM.

best regards,
g.f.

  • Hi g.f.,

    Two considerations for using the EVM as a master clock

    1. Check out the app notes on implementing a master using DP83640. In those app notes you'll see that an accurate PHY ref clk is needed. On the DP83640EVM, we use a regular 25MHz crystal. This is not ideal.

    2. The PTP stack still needs to run in higher layers. You will need to connect the EVM to a MAC using the MII connector.

    The EVM is capable of being a master clock, but those 2 points need to be taken into account.

    Best Regards,