Other Parts Discussed in Thread: XIO2213B
I know the XIO2213B does not support Message Signaled Interrupts, but does it support Legacy Interrupts (in-band messages) ?
Legacy Interrupts: In PCI Express, four physical interrupt signals (INTA-INTD) are defined as in-band messages. When the core needs to generate a legacy interrupt, it sends INTA-INTD message upstream which would ultimately be routed to the system interrupt controller.
From the XIO2213B datasheet:
3.4 PCI Interrupt Conversion to PCIe Messages
The bridge converts interrupts from the PCI bus sideband interrupt signals to PCIe interrupt messages.
Since the 1394a OHCI only generates INTA interrupts, only PCIe INTA messages are generated by the
bridge.
Is there any information you can provide on how to configure the XIO2213B evaluation board to generate the generate these interrupt PCIe messages ?
Thanks,
Marcin