This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About XIO2001EVM external compornent

Guru 19685 points

Other Parts Discussed in Thread: XIO2001EVM

Please let me know about external parts of XIO2001EVM.

①L3:Inductor or Filter

 ・XIO2001EVM user's manual written in L3:"200Ohm 200mA"(page 21: schematic), but BOM list is 10μH inductor.

  Which is correct? (Is BOM list typo?)

 ・If filter is correct, is L3 use BLM21(same as L1 & L2) no problem?

②EEPROM

 ・Is there information of EEPROM data format or writing method?

 ・XIO2001EVM is connecting 24LC08BIST(I2C 8Kbit) EEPROM.

  Is EEPROM change 4kbit device no problem?

 ・If the case of unused EEPROM, I will connect GPIO4/SCL to pulldown.

  Is there any other careful point?

Best regards,

Satoshi