Other Parts Discussed in Thread: DS90UB914A-Q1
I would like to confirm how to set the commands and the setting data by I2C commnication for DS90UB913A/914A-Q1.
The customer wants to use DS90UB914A-Q1 and 913A-Q1 for the camera module. They will use them by Figure 4 of SNLA222 and tried to do it but
they could not be operate them. They can not understand I2C control.
And they can not use GUI for EVM because 1.8V interface.
I have questions for it.
1. Do you have the sample program for I2C communication?
2. If you don't have it, could you please advice the setting for sending commands by I2C from the master (the side of DS90UB914A-Q1)?
ex) how to set the command in DS90UB914A-Q1, the steps for the sending the command, the caution of the setting (data, clock, and so on)....
Best regards,
Atsushi Yamauchi