This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6424ARGJR I2C IO Expander, schematic check



Hi. I'm about to build an LED indication board (to be used for debugging another board) based on the TCA6424ARGJR. Is this schematic OK?

Specifically, is it OK to leave the INT pin floating? If I don't plan to use the RESET pin, is it OK to connect it to VCCI like this with the pull up resistor? I will have pull up resistors configured in the main processor on the other board for the SCL and SDA lines, so is it OK not to have any on this end?

LED-board.pdf