Other Parts Discussed in Thread: DS15EA101
Hello,
My customer has a question about DS15EA101.
My understanding is as follows.
- The input signal amplitude must be 800mVppd +/- 10% (VID=400mV +/- 10%) because its automatic equalization circuitry is dependant on the signal amplitude.
- The optimal amplitude is VID=400mV.
- Any deviation from the optimal amplitude in either direction will cause the equalizer filter to assert either excessive or insufficient amount of gain as illastrated in SNLA112E Figure 2.
[Q]
For example, Does VID=400mV +/- 10% mean the part which I showed as follows in datasheet Figure 15?
Best Regards,
Hiroshi Katsuanga