Other Parts Discussed in Thread: DS100MB203
We are using DS100MB203 and controlling it's operation with the SMBus (not pin mode). We have register 08 set to a C (bit 2 =1) and register 2D set to A8 (bit 6 = 0). As I understand the datasheet this should set the device in PCIEGen3 MODE, which should put the outputs in "transparency mode".
My question is - does "transparency mode" mean that the output controls for VOD (2D bits 2:0) and DEM (2E bits 2:0) have NO EFFECT on the output? The ouput should just follow the signal seen at it's input?