This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding the usage of PECL drivers and receivers TB5D1M and TB5R1D

Other Parts Discussed in Thread: TB5D1M
We are planning to use the PECL based Driver IC and Receiver IC in our ATE application.
Part Number we have chosen are TB5D1MD for PECL driver and TB5R1D for PECL receiver.
We need clarification from regarding the usage of these IC's which we are planning to interface it with the IC part MC10ELT28DG available in our customer module.
Problem we are observing is the difference in the input and output voltage level of these IC's (Voh, Vih, Vol and Vil). Can we interface these IC's with standard PECL level IC's? Any additional care to be taken for interfacing.
 
The below difference (in table) I am seeing with Voltage specifications of Standard, MC10ELT28 part and TI parts. Request to provide a solution
Sl.No Standard PECL Input and Output Levels (VDD : 5V) Specification on our Customer IC MC10ELT28 (VDD : 5V) Specification of TB5D1M PECL Driver (VDD:5V) Specification of TB5R1D PECL receiver (VDD : 5V) Units
Parameter Symbol Min Max Min Max Min Max Min Max
1 Driver High Voh 3.98 4.12 4.02 4.19 VDD – 1.8V = 3.2 VDD – 0.8V = 4.2 -   V
2 Driver Low Vol 3.19 3.38 3.05 3.37 VOH – 1.4V = 1.8 VOH – 0.7V = 3.5 -   V
3 Receiver High Vih 3.84 4.12 3.87 4.19 -   2 - V
4 Receiver Low Vil 3.19 3.52 3.05 3.52 -   - 0.8 V