This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Initilization code for DP83848 Interfacing with IMX6 processor



Hello All,

              I am Interfacing  DP83848 with IMX6  Processor.Processor is single core,1 Ghz. I am doing this interface in RGMII Mode i.e trigger based interfacing. is there any Initialization code  necessary for this? if yes kindly share the link or suggest the solution.

  • Hi Dushyant,

    The DP83848 does not support RGMII.

    They new DP83867 does though. For using any of our PHYs, you can use hardware bootstraps to change PHY features. The PHYs we make do not require any special initiation unless you want to use a specific feature or mode.

    Kind regards,
    Ross