Other Parts Discussed in Thread: SN65HVD251
We're using the SN65HVD251DR as an CAN interface on our Battery Monitor device. We had a failure where the Rx pin on the logic side failed.
The Rx pin is connected to 390ohm resistor to the Cathode of the LED of a 6N137SM optocoupler.
The Anode of the LED is connected to the output of a TI part# DCP010505BP-U/700 DC/DC isolator which is not outputting +5V but 6.1V probably due to not being heavily loaded.
The SN65HVD251 is also powered by the DCP010505BP-U700 so its getting 6.1V on its Vcc pin could this cause a failure on the Rx pin?
Thanks,
Ed