Other Parts Discussed in Thread: DS10CP152
Hello,
Cross-talk is output from OUT0 in my prototype board using DS10CP152.
When IN0 is a clock signal,Cross-talk is not output.
Is there something that is considered to be the cause of this cross-talk?
Could you give me some advice about this?
○Configuration:
SEL0:1,SEL1:0 (OUT1:IN0,OUT0:IN1)
EN0,EN1:1 (OUT1:Enable,OUT0:Disable)
○Input Signal:
IN0:pseudo-random signal
IN1:Differential 0V,Common mode voltage 1.34V
○Circuit Connection:
Decoupling capacitor:10uF,0.1uF,0.01uF
IN0:LVDS Driver Output
IN1:Pulse transformaer(The primary side is floating,the secondary side is pulled up with 6.8kΩ and 10kΩ)
OUT0:LVDS Receiver Input ←Crosstalk is output
OUT1:Pulse transformaer(The secondary side is floating)
Best regards,
Seishin