This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need a GPIO expander to replace PCA9571GUX

E2E,

I’ve a request to cross ref - NXP PCA9571GUX -> http://www.nxp.com/documents/data_sheet/PCA9571.pdf.  Would you please recommend the best replacement? 

Thank you,

Adam

  • Hello Adam,
    Does it have to be a functional cross or does it have to have the same foot print too?
    -Francis houde
  • Hello Francis,

    Please provide both.

    Thanks

  • Vincent,

    Please see the following selection chart:

    Just for more clarity I'll explain some of the features I state in the chart.

    RESET

    Some I/O expanders feature a RESET pin, which offers the ability to manually reset the device using a microcontroller/microprocessor to toggle this input.

    Internal Pull-ups

    Internal pull-up resistors has the benefit of saving both board space and placement costs for external resistors. Internal pull-ups are more useful for applications where several or all of the ports are set as an input and require pull-up resistors. Since the pull-ups are connected to VCC, increased power consumption will occur when the inputs are held at a low state.

    Hope this helps!

    Siby