The subject part includes a Fail-Safe feature. Page 14 of the datasheet (just above Figure 25) says, “The fail-safe feature uses an AND gate with input voltage thresholds at about 2.3 V to detect this condition and force the output to a high-level regardless of the differential input voltage.”
Is the output only driven to the high-level if the applicable EN pin is in the high state (i.e. a given output only goes high in fail-safe mode if that output is enabled).