Dear all,
We're working in RMII mode with a DP83848.
As it's mentionned in the datasheet (page 15 ; table 2-7), the pin 39 (RX_DV/MII_MODE) must be tied to high and pin 6 (SNI_MODE/TX3) must be tied to low to be in RMII mode, I have done this.
Moreover, pin 40 (CRS_DV) is directly connected to my microcontoller.
With that, my Ethernet connexion doesn't work properly. But When I connect pin 40 to pin 39 (so pin 40 is tied to high), it's works perfectly, I have Ethernet communication, my modbus TCP works fine.
So, I don't really why it works in this case.
If somebody can help me to understand.
Thank you,
Regards,
Fabrice