Other Parts Discussed in Thread: TPS2042, TUSB2036
Hello,
I have a problem with the TUSB2036 in combination with the TPS2042. My upstream device is a 'PICO-IMX6-EMMC' system on module.
I've connected it much like the schematic in '6Mhz Bus-powered 2-port hub.pdf' from the reference schematic.
But when i power on the PICO my usb devices won't work. I don't measure 5 volt on the out1 and out2 pins of the TPS2042 and the /EN1 and /EN2 pins are always high. However, the suspend pin on TUSB2036 is low.
Is there something wrong with my schematic? I've included it.
Hope you can help, thanks in advance.
ArendUSB Schematic.pdf