Hi,
For DP83867 do the SGMII_SIP and SGMII_SIN pins require an external 100 ohm differential termination resistor?
In table 2, note 1 says that internal pull-up and pull down resistors are disabled when the device enters functional mode. Section 7.1 says I should pull all unused inputs up or down. What is the point of pull-up and pull down resistors on non-strap input pins, such s TX_D3, if they go away after the device enters functional mode? Are they really disabled?
Also,
Besides a reduction in power, is there any advantage to using an external 1.8V supply with this device.
Regards,
David