Other Parts Discussed in Thread: TPS65982, TPS65982-EVM, HD3SS460, TPS6598X-CONFIG
Hello TI,
My customer is planning on using the TPS65982.
Per the Customer:
We are receiving embedded display port over a USB C connector. We have a Parade Semi PS8742 to handle the video conversion.
Our setup is a MacBook Air and a LG 27" 4K display. We can connect the MacBook to the display directly and it works. We can go through an external commercial USB-DP adapter and it works.
What I can't get working is taking the TPS65982EVM and the Parade Semi PS8742 EVM to display video. I have the two CC lines connected between the two boards, and the TI EVM is receiving power from the Parade EVM.
I have the switches set up as 0010 and I see LED A on solid which is correct for DP Alternate mode, and the Consume LED is on.
I see communications over the CC bus, sensible BMC signals.
If there is any advice on how to debug this problem I would appreciate it.
Thanks,
Dan