Other Parts Discussed in Thread: TPS65982
Hi team
I found the TPS6598x OCP function is abnormal when setting Peak current to 130%, 150% and 200%. But the OCP function is normal if peak current=100%.
For example,
Case1:
Set the Source PDO0 = 5V/3A, PDO1=12V/3A, PDO2=20V/3A and set the peak current=130%.
Then we use a DC load(CC mode) on VBUS to sink the current. We found the TPS65982 not turn off the VBUS even the output current over 5 Amp.
Case2:
Set the Source PDO0 = 5V/3A, PDO1=12V/3A, PDO2=20V/3A and set the peak current=150% or 200%.
Then we use a DC load(CC mode) on VBUS to sink the current. We found the TPS65982 turn off the VBUS when the output current just 1.1 Amp.
I use GUI2.7 and GUI2.8 to gen the bin and test on TPS65982 EVM, the symptom are the same. Could you help to assign someone for take a look?
Eric