Other Parts Discussed in Thread: SD384EVK, LMH0384, LMH1219
Hello,
I'm using the SD384EVK to evaluate the LHM0384 and had a quick question regarding the SDI rate of the LMH0384.
I just wanted to ask per the datasheet that the maximum input data-rate was specified at 2.97 Gbps. This is ~1.5 GHz for falling and rising edge. Does this mean I can feed into the input of the LMH0384 a signal of up to 1.5 GHz?
I am asking this because I can only go as high as 950 MHz into the input of the LMH0384 (SDI). There is no mentioning of maximum input frequency in the datasheet (just maximum DR of 2.97 Gbps), so I may be misinterpreting things.
Regards,
Hayden