Other Parts Discussed in Thread: TPS65986EVM, HD3SS460, DP-EXPANSION-EVM
Is there any known compatibility issue between the TPS65986EVM + the DisplayPort Source board, and the Apple USB-C Multiport adapter?
Using the EVM firmware along with the switch S1 set to Add-In card) the HDMI video output works on the Apple USB-C adapter, but USB-A port doesn't work on it. I have the power supply going to the TPS65986EVM, and I have the type C power port on the apple adapter left unconnected (the multiport adapter works fine as sink).
If I use the TPS6598x Application customization tool with the TPS65986_HD3SS460_DFP_Full_2_8.tpl settings then the USB port works, but not the Displayport. The monitor is detected by the computer, but when I try to extend the video to that monitor it says "unable to save display settings. I tried another computer as well, but that didn't work either. It didn't display an error message, but the video never got enabled so it went back to the previous settings.
I can't understand why the Displayport works with the EVM firmware/settings, but not with the flashed App firmware from the customization tool. I logged the CC data with a CC sniffer, but I don't see any obvious differences.
I'm really having a hard time finding a good starting point to work from. If I use the EVM firmware I typically get expected results on both sides (not counting the apple adapter). But, I need to be able to customize the settings and I don't see an easy way to do that with the EVM firmware/settings. So I've been using the example projects, but they don't seem to work as well as the EVM firmware even before I attempt any customization.
What I'm ultimately trying to do is to create two sets of firmware. One for the DFP side that is dual-lane displayport, USB 3.1g1, and 20V@3A power delivery. The other is for the UFP side that is the sink for the Displayport, power, etc. I'm only using the Apple USB-C multiport adapter because it's a 2-lane device with a USB 3.1g1 port.