Hello,
I have some questions about the Dual PHYTER DP83849IFVS.
We tried to use the DP83849IFVS as a Media Converter by putting the Pin EXTENDER_EN on high level (2.2k pull up to 3.3V). We also did some configurations with the Pins AN_EN, FX_EN and so on. Like its described in the Application Note / Datasheet.
My question is: Is it necessary to do some configuration of the registers to let the PHY work as a media converter? We have a MSP430 LaunchPad where we can read/write the registers of the PHY with the software USB2MDIO. Or is it enough to do the right configuration with high/low levels at the input pins of the PHY?
In addition some information about our application:
- We want to use the PHY as a media converter to convert the ethernet signals from IEE standard “TX” (electrical) to IEE standard “FX” (optical)
- On PORT A (TX), a RJ45 is connected
- On PORT B (FX), an optical transceiver is connected
Thanks for your help.
Michael