Other Parts Discussed in Thread: TMDS181
I'm using the TMDS181 Evaluation board, and for the most port it works well, however when I use the OpenHour Chameleon 4K media player as a source and a Samsung LU28E590DS UHD monitor, it blinks when trying to display 4K60. I've played with as much manual settings as possible as well as the default pinstraps (I2C_EN low, J3 -> 2-3). I find the default pinstraps works best, and if I configure the Media player to output 1080p60 I get a nice stable image, I then change the resolution to 4K30, and I get a stable image, then I go to 4K60, and half the time I get a stable image, the other half the time I get a blinking image, but for some reason the TMDS181 eval board works best when I first start at 1080p60 and walk up to 4K60. If I directly connect the media player to the monitor it's fine.
We have 4K pattern generators, PCs and other monitors that work fine with the TMDS181, it's this combination of the Chameleon media player and the Samsung monitor that is giving me problems.
Any ideas or recommendations would be much appreciated.
Thanks,
Michael