Other Parts Discussed in Thread: TUSB8020B
Hi Bros,
My customer using our TUSB8020B in dual camera solution. The block diagram is below:
Now, only one video signal can be got at PC. Now, I guess the issue may comes from:
1. When the upstream port is connected to an electrical environment that only supports high-speed or full-speed/low-speed connections, SuperSpeed USB connectivity is disabled on the downstream ports. When the upstream port is connected to an electrical environment that only supports full-speed/low-speed connections, SuperSpeed USB and high-speed connectivity are disabled on the downstream ports.
2. Over current at OVERCUR1z
3. register config problem.
Do you have any suggestions what should I do when I met the problem? Like testing which points' waveform or how to identify the problem? Many thanks.