Other Parts Discussed in Thread: TPS65982
Hi Team,
Customer found TPS65982 0x5F bit 3 overcurrent is still 0b when there's overcurrent event
Either of below sequence the overcurrent bit is still 0
1. When TPS65982 as source and VBUS = 5V, short VBUS to GND. Then 0x5F bit 3 = 0b
2. TPS65982 set as DRP, Connect VBUS to GND with 0.89 ohm resistor, then plug in another UFP device. See VBUS = 0V, 0x5F bit 0 =1b, but bit 3 = 0b
Could you help check? Intel feedback to customer Alpine Ridge is checking 0x5F bit 3 to report overcurrent event, but currently TPS65982 is not function correctly
Thanks
Sam