Other Parts Discussed in Thread: AM26C31, AM26LV31E
Hello
I am using AM26C31 RS422 driver and i need to interface it with my 3.3V microcontroller (stm32f427).
AM26C31 works in +5V supply. So do i need to use any level translator between AM26C31 and uController?
AM26C31 has voltage levels:
VOH 2V min
VIL 0.8V max
And STM32f427 has levels:
VOL 0.4V max
VIL 2.9V min
thanks
Azeem