This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVS885 fail indicate

Other Parts Discussed in Thread: SN65HVS885

Dear Sir 

Customer would like to do short detect ,if input short to GND,we can indicate low or high to MCU

Could SN65HVS885 support this feature ,do you have recommend solution ??

  • Hi Kai,

    If the parallel (field) inputs of the SN65HVS885 device are shorted to GND, the input voltage would fall below the low-level input threshold value (4 V minimum). So, the state of that input would be reported as a logic low level when read out on the serial interface (SOP). This would be the same behavior as if the input were driven low normally (by some input device on the field side).

    Let me know if you have any other questions or if I mis-interpreted what you were asking.

    Max